This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24616充电问题

Other Parts Discussed in Thread: BQ24616

正在调试BQ24616充电,使用输入20V,充电电压4.2V(1S),Idmp=2A,Iprechg=0.3A,Ichg=1A,在不接电池的情况下,PH输出如下图所示:

当连接电池之后,PH波形如下:

到最后,PH输出恒定的3.8V,和电池一样一致,拔掉电池之后PH波形又恢复到图1波形,输入端电流一直在0.01-0.02之间变化,无任何充电电流,查看STAT1和STAT2状态灯都是正确的,这个是什么原因导致的?

为什么接入电池之后PH就不工作了呢?是反馈哪里出现问题了吗?