目前設計是照DEMO的線路來作,關於這顆POWER IC有以下幾點問題:
1.想請教一下關於LM25118這顆POWER IC是否有OCP的功能?
2.如果有OCP,那麼OCP應該如何計計?
3.在SPEC上所求的Iripple以及Ipk是對電感端的電流,還是輸出IOUT就是照那部分所寫的使用?
關於這幾點麻煩當忙解答,謝謝.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
目前設計是照DEMO的線路來作,關於這顆POWER IC有以下幾點問題:
1.想請教一下關於LM25118這顆POWER IC是否有OCP的功能?
2.如果有OCP,那麼OCP應該如何計計?
3.在SPEC上所求的Iripple以及Ipk是對電感端的電流,還是輸出IOUT就是照那部分所寫的使用?
關於這幾點麻煩當忙解答,謝謝.
LM25118是一顆寬電壓buck-boost 電源控制晶片
1. Yes, LM25118 has OCP
2. The OCP level will be set by the resistor between pin CS and CSG. Details of calculation can be followed by the equation in page 20 of the datasheet(R13 calculation).
3. The Ipk and Iripple refer to Inductor current(電感電流)
祝設計順利
We may have different versions of datasheet or pdf format, yes, pls refer to R13 calculation in LM25118 datasheet.
請注意LM25118的OCP是PEAK current mode.
同時因為LM25118有buck mode 和 buck boost mode 因此Ipk 皆需計算取較大值已確保電流輸出
另要注意的是在buck boost mode 時 current limit threshold 會自動設定為2倍
首先需確認你的6A是continued load current 還是peak Inductor current.
假設是continued load current(Iout) 則請依照equation 10 至 equation 13 即可計算出所需R值
請注意 LM25118 的 OCP 是 Hiccup mode 而不是shut down. 優點是過流解除就會自動回復
1.假設是在 peak inductor current(OCP)=6A(buck-boost mode) vin=9 vout=12,
equation:6=Iout(1+12/9)→Iout=2.6A? 是嗎??
2.set CCM Iout=3A calculation R=25m ohm Ipk=10A(Buck-Boost mode) so OCP=Ipk(Buck-Boost mode)=10A or
OCP=auto double Ipk=20A?
Thanks.
若buckboost mode Ipeak 為9.5A,
則依據equation 13, R13=2.5V/(10*Ipeak)=26mohm
1. 通常在設計上我會用Iout去推算出Ipeak意以用來設定peak current limit
2. Don't be confused bu the double limit, when you set Ipeak for buckboost mode then it follows your setting. when calculating R13, if use buck mode Ipeak the reference voltage is 1.25V and when you use buckboost mode the reference volatge is 2.5V. Pls refer to equation 12 and 13.
When you calculate R13 based on buckboost current with reference voltage of 2.5V
the Ipk OCP under buckboost mode will be just as what you set(in this case 9.5A).
Only if you calculate based on buck mode Ipk with reference voltage of 1.25V, the OCP under buckboost mode will be double to what it is under buck mode. Hope this help.