This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76PL455采集问题



各位好:

     跑路试过程中,出现455采集异常问题,表现为温度采集正常,通讯正常,所有单体电压为0情况,持续时间为40S,(目前只有一块板出现这样异常情况)
请问什么情况下会导致这样现象出现?
  • Hi,

    关于您的问题,咨询了相关产品线同事,这种情况之前没出现过,所以希望你那了解更多信息,如下:
    您能否提供有关board/setup的更多信息,并阐述IC的状态吗(它在此期间是否进行任何电池平衡或其他操作)? 测试了多少其他未显示故障的电路板? 它在一块板上是可重复的吗?
    您也可以直接和他交流,链接如下:
    e2e.ti.com/.../2753201

    Best Regards,
    Sherry
  • 也遇到过类似的问题。长期数据监控过程中,发现有时某一个BQ76PL455采集板传回的电压数据通过了CRC校验,但是16个电压采集通道中,部分通道电压为0V,部分通道电压为4.9V左右,接近5.0V。该现象发生频率很小,半年我们一共在2个实验平台上分别发现过1次。