This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24610每次只能充10分分钟左右停止充电



TI你好!

         我的电路设定适配器输入电压26V,充电电压设定25.2V,快充电电流设定2A,预充充电电流160ma

状态都很好,就是每次接通电路只能充10分钟STAT1灯即灭掉,STAT2灯并没有转亮,测试电池电压也未到设定电压。断开充电器,再连接可以再次充10分钟左右,如此循环.....

       以上情况测到TTC脚电压为1V,VREF电压3.3V,CTTC电容按手册用0.056uf。

      请协分析:1.TTC电压1V是否正常

                        2.如果是安全定时器记时异常,是什么导致的。

以上情况,请协助分析,提供对策方案。谢谢