TPS51200的EN脚,我只知道高时,VO有正常输出,低时discharge。对于suspend to ram 这种用法我不理解。我使用这个芯片的目的是给DDR3L的VTT供电,这款DDR3L是MT41K256M16TW。要使用suspend to ram功能,我的EN如何连接呢,连接到片选信号?
谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TPS51200的EN脚,我只知道高时,VO有正常输出,低时discharge。对于suspend to ram 这种用法我不理解。我使用这个芯片的目的是给DDR3L的VTT供电,这款DDR3L是MT41K256M16TW。要使用suspend to ram功能,我的EN如何连接呢,连接到片选信号?
谢谢。
Hi,
S3是计算机工作的一种待机状态,这种状态下的系统是suspend to RAM的,即内存仍然保持供电状态,保存着运行数据。计算机主板上是和芯片组负责给出S3控制信号的引脚相连,一旦操作系统命令进入S3待机状态,VDDQ与VTTREF仍然有电,而VTT会关闭。
如果你的系统不是计算机系统,没有专门的S3控制信号,我觉得与CS相连也不应该。因为一旦你启动写入或者读取,先使能片选,很快就会进行写入读取,这是已经需要VTT正常工作了。这很短的时间VTT供电来不及启动。所以我认为还是应该和专门控制S3待机的信号相连。
谢谢!