参考TI官方手册,设计了TPS55340升压电路,输入4.8V,输出6V,开关频率为470kHz左右。当空载时,噪声达到300mV,带1A的负载时,噪声达700mV,其中空载时,发现尖峰噪声的频率约为470kHz左右,这个频率恰好是开关频率,不知道是怎么回事?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
参考TI官方手册,设计了TPS55340升压电路,输入4.8V,输出6V,开关频率为470kHz左右。当空载时,噪声达到300mV,带1A的负载时,噪声达700mV,其中空载时,发现尖峰噪声的频率约为470kHz左右,这个频率恰好是开关频率,不知道是怎么回事?
Hi,
对于boost电路来说,高dI/dt的关键路径是SW -- Diode -- Cout+ -- Cout-(PGND) -- PGND -- MOSFET(集成在芯片内部) -- SW.
对于这种集成boost converter,具体来说,就是从SW出发,到diode,到输出电容,到输出电容的地,到芯片的PGND,形成的环路面积要最小。看你的layout,这个环路面积比较大。应该是把二极管掉一个方向,然后把输出电容横跨在左下角芯片PGND和二极管输出一端之间。
谢谢!