This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
用负载仪测试BQ24614的充电输出,充电电流只有0.12A,实际设置为2A
您的电池电压是多少?
我现在是用电子负载仪测试,设计的充电电压为21V,输入电压为24V,充电电流为8A,输入电流限制为10A,预充电流0.3A
打开电子负载,电压显示19.5~21跳,负载仪输入电流设置为0.12A,打开负载仪,芯片就保护了。低于0.12A就正常。