This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24616充电异常

我按照参考设计,设计了自己的底板,输入电压为24V,充电电压为21V。设置为输入电流4A,充电电流3A,prechg电流0.3A,测得ISET1电压为0.6V,ISET2电压为0.3V,ACSET电压为0.8V。

用电子负载仪连接到充电口,设置负载仪输入电流为0.1A,打开电源,电子负载仪显示电压为21V,打开电子负载仪输入,正常。逐渐增加负载仪输入电流,当电流为0.12A,芯片动作保护,无输出电压,电流为0。

其他参数均与参考和计算工具内的参数一直。