This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求推荐一款LCD供电(背光供电、VGH VGL VCOM等都有)芯片



大家好:

    我最近准备用一款LCD,想找个供电芯片,最好能把背光供电、VGH VGL VCOM都能提供的;这款屏上面需要接的电压大概如下所示,不知道TI有没有这种专业的供电芯片,最好能提供较多的如下电压,用的芯片越少越好。大家谁熟悉这块,麻烦推荐一款合适的供电芯片。

1、背光电压:9.0-10.5

      被光电流:160mA

2、栅压

     VGH:18V

     VGL: -6V

3、模拟供电

      AVDD:9.6V

4、供电

     VDD: 2.8-3.3

5、COMMON电压

      Vcom: 3.2V