This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

回复: 电池电量

求专家回复

  • 看到TI的测试数据,现在的Li电池主要有四种:

    LiCoO2 - Coke:   3.0V to 4.1V

    LiCoO2 - Graphite:   3.0V to 4.2V

    LiMnO4 - Graphite:   3.0V to 4.4V

    LiFePO4 - Graphite: 2.0V to 3.6V

    这四种的充电电压、OCV与电量的曲线也都不一样。

    那么,对于同一种类型,比如现在比较常用的LiCoO2 - Graphite,不同厂商生产的同类电池,其OCV与电量的曲线关系会有不同吗?

    TI的用于系统端的电量计IC,如BQ27520是如何对不同电池进行区分的?是否支持如手机类型的可更换电池的应用?

    求专家回复