在初次使用LM26003时,很疑惑,为什么没有输出电压?设计初衷是想输入12V,输出3V,50mA。焊好板子后,没有负载,刚开始时3V,以后就变成5.8V,然后就下降到0V,当再次上电,电压就在0V~~5.8V之间了,最后没有了。请问这些是什么原因啊???
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
请确认一下续流二极管是否虚焊?
另外,如果您的输出电流仅仅只是需要50mA ,不推荐你采用LM26003, 它适合较大电流输出的降压设计,当负载较小是效率比较低。
推荐TPS62125,见其官方网站:http://www.ti.com.cn/product/cn/tps62125 , 5mA以上都可以达到88%左右效率 。