This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51216 S5 pin ABSOLUTE MAXIMUM RATINGS

Other Parts Discussed in Thread: TPS51216

dear all,

  

最近在使用TPS51216 但是在使用的时候 测试S5 pin Undershoot电压为 -0.896mV t不超过5ns。

但是IC Spec ABSOLUTE MAXIMUM RATINGS只标注了-0.3V~6V,没有提到时间

所以想咨询下这个信号undershoot是否有风险呢?谢谢!