你好,新做样机输入390V,输出20V 60A。老化2小时断电冷却后重新上电带载开机时出现炸管,检修发现变压器初级电感由之前700uH变为370uH.初步判断为变压器老化损坏。请教出现此故障的原因是电路设计缺陷还是变压器本身质量问题。附件是UCC3895原理图.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,新做样机输入390V,输出20V 60A。老化2小时断电冷却后重新上电带载开机时出现炸管,检修发现变压器初级电感由之前700uH变为370uH.初步判断为变压器老化损坏。请教出现此故障的原因是电路设计缺陷还是变压器本身质量问题。附件是UCC3895原理图.
变压器温升确实很高,今天将另外一台机器老化了一个小时左右表面温度103度左右,不知道是不是我的变压器设计不合适。附件是样品变压器规格烦请大家帮忙分析,谢谢!
100多度的话,EE55磁导率会变低吧?··那样同样的输出条件要求匝数会变大吧,如果是高要求的产品可以试试纳米基材料的磁心··其温度特性很好··
如前面所说,你要看一下你磁芯的特性曲线,看在高温下相对磁导率是如何变化的,变化幅度多少?然后考虑一下,电感变化对你电路的影响。还有你是不是垫气息了?为什么垫这么大气息?感觉这么小电感值气息会比较大。
你的变压器匝比是10:1,对于最高输出24V来说,占空比才60%是不是小了点?还有就是你的电感,我觉得没必要那么小,电感的大小与轻载时候的稳定性有什么关系呢?