Other Parts Discussed in Thread: DRV8353R, DRV8353RS-EVM, MOTORWARE
使用DRV8353R官方开发板DRV8353RS-EVM,接自己的电机进行空载测试,使用几分钟就出现硬件FAULT灯亮,通过SPI总线显示为GDUV故障。更换芯片使用一段时间后仍然出现该故障,请问故障原因是什么?是否有相应的解决方法?或者需要进行何种保护以避免这种问题?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: DRV8353R, DRV8353RS-EVM, MOTORWARE
使用DRV8353R官方开发板DRV8353RS-EVM,接自己的电机进行空载测试,使用几分钟就出现硬件FAULT灯亮,通过SPI总线显示为GDUV故障。更换芯片使用一段时间后仍然出现该故障,请问故障原因是什么?是否有相应的解决方法?或者需要进行何种保护以避免这种问题?
我在使用DRV8353RS-EVM时遇到了类似的问题:使用motorware的代码,将isink和isource改到2A和1A,PWM频率改到35K,驱动T-MOTOR U5 400KV电机,在18V输入,1K RPM 轻载的情况下运行了两分钟,fault亮灯,检查DRV8353RS的寄存器发现出现GDF错误,即gate driver fault;测量GS电阻发现C相上桥电阻较小,12.8Ω,其余桥路正常,为142K;取掉MOS后电阻不变,推测DRV8353R的栅极驱动损坏。
个人认为该片子目前还不太稳定可靠,相比于DRV830X系列预驱能力有所削弱,建议等正式版芯片出来后再进行进一步测试。
我最近也买了一片8353RS,准备制作8000瓦的FOC,一起交流下,盼复