This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53681通过PMBus指令设置VID电压无PWM波输出

Other Parts Discussed in Thread: CSD95490Q5MC, TPS53681

您好,我们正在调试TPS53681,它有望通过PMBus命令控制A通道输出PWM1 / PWM2 / PWM3并通过三个CSD95490Q5MC芯片获得0.42V电压,现在IIC读/写寄存器都可以, 我的配置如下流程:0X00寄存器设置为0X00,0X03寄存器设置为0X00,0x04寄存器设置为0x02,0x01寄存器设置为0x80,0x02寄存器设置为0x1B,0x24寄存器设置为0x0029,0x2B寄存器设置为0x001B,0x21寄存器设置为0x001D,其他寄存器使用其默认值,但在TPS53681输出端点没有测量到PWM,所以现在我需要了解操作流程如何由TPS53681通过发送PMBus命令输出预期PWM,或者是否有相应的开发DEMO代码,希望回复,谢谢。

  • Hi
    TI有评估板: www.ti.com.cn/.../sluubp7.pdf 但是你需要购买,或者找你们常购买芯片的授权代理商,看能否借用一下。
    或者你按照你的配置,但是按照EVM板的操作看看(在EVM板配置部分,改为你的配置,其他按照其步骤操作)