This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

电量计学习过程————放电截至电压的设置



问题1:学习过程中有一步是放空电池的电量,我想问下比如,我在老化柜设置的放电条件是0.2C放到3V,可是查看记录的log文件显示RSOC在此时只放到了1%或者2%,没有到0%,这影响Qmax和FCC更新吧?

我是不是应该把截至电压再往下调低一些,比如2.9V,让RSOC显示0%。

客户给的规格书里写的单节电池放电保护电压是2.7V,恢复电压是2.9V。

还是说把放电截至电压调到2.7V。

问题2:如果客户手里使用时并没有达到学习时的放电截至条件,会不会导致几个循环后,FCC和Qmax下降很快的现象?

期望TI的工程师帮忙回答下这个问题,非常感谢。