四节(或以上)锂电池并联,20AH容量
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
可参考下BQ2419X系列的充电器:
ok,多谢。
另外,还想选用一款ti 的升压芯片,输入为单节锂电池(2.8V-4.2V),输出为6V,3A
最好为内置mos,如果没有内置mos的,可以采用外置mos,要求电路尽可能小(尽量不采用QFN封装)
另外,对于多节并联的锂电池,BQ2419X是否要每节电池都加一个还是说多节可以用一片BQ2419X充电?
如果用一片,那么每节电池的过充过放如何保护?(换句话说就是如何避免其中的某节电池在充电的时候已经过充,但是还有的没有充满。放电亦是如此)