This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-01599:在变速驱动实现扭矩安全关闭功能的方案中,使用TPS27S100的优点有哪些?



在变速驱动实现扭矩安全关闭功能的方案中,使用TPS27S100(单通道高侧开关)的优点有哪些?

TIDA-01599是TI的一个参考设计,可在变速驱动中实现扭矩安全关闭的功能 (依据IEC61800-5-2)。

TPS27S100是一种单通道高侧开关,用于开启/关闭隔离IGBT栅驱动电源,从而实现扭矩安全关闭(STO),其优点如下:

  • 开启/关闭信号与LVCMOS/LVTTL信号兼容;
  • 可以选择限制和监测由隔离IGBT栅驱动电源产生的电流,有助于监控电源的健康状况以及输出端的故障检测。
  • 3.5-40 V的宽范围工作电压,可支持控制栅驱动电源供电(5-24 V ±20%),为额定电压提供了足够的安全裕度。

关于这个主题更多的信息, 请参考User Guide for TIDA-01599的第2.6章节 " System Design Theory " 。你也可以从TIDA-01599 folder,下载更多的参考设计文件 (BOM, 原理图, Gerber) 。