我在使用TPS65217D为AM3352供电
希望,接入外接电源后,TPS65217D能够直接启动。
请问,这样子该如何设计TPS65217D的PB_IN引脚呢?
我在看TPS65217D的手册时,发现,都把这个引脚接上了一个按键,但是,我的系统中,不能用按键。
那么,怎么设置TPS65217D的PB_IN引脚,不接按键,上电能够直接将启动呢?
谢谢!
可以直接下拉接地吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我在使用TPS65217D为AM3352供电
希望,接入外接电源后,TPS65217D能够直接启动。
请问,这样子该如何设计TPS65217D的PB_IN引脚呢?
我在看TPS65217D的手册时,发现,都把这个引脚接上了一个按键,但是,我的系统中,不能用按键。
那么,怎么设置TPS65217D的PB_IN引脚,不接按键,上电能够直接将启动呢?
谢谢!
可以直接下拉接地吗?
不能直接下拉到地,因为连接GND超过8s,就会重启,还是建议加一个开关按键用来起机吧,除非你有外接一个MCU的I/O pin去控制它的高地电位
From the OFF state (going to the ACTIVE state):
• Push-button is pressed (falling edge on PB_IN) OR
• USB voltage is asserted (rising edge on USB) OR
• The AC adaptor is inserted (rising edge on the AC pin)
我看到芯片手册里面这么描述的,
那么可以悬空这个PB_IN引脚或接一个电容到地,
这样可以实现TPS65217D在USB或AC上电后直接启动?
谢谢~
芯片的启动需要有一个拉低的动作,你接了电容,这个管脚始终没有拉低的动作