问题1.MOSFET的驱动峰值电流按以上图片I=Qg/td(on)+tr和I=Qg/td(off)+tf算下来的电流区别还很大,I=Qg/Ton,这边的Ton是按什么算?
问题2.MOSFET参数Vgs th-栅源极阈值电压5V,Vgs - 栅极-源极电压30V,选驱动芯片的驱动电压最小为多少,最大为多少V?
问题3.MOSFET的耐压值400V,电流Id为17A,满足这条件的MOSFET常用型号有哪些?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
问题1.MOSFET的驱动峰值电流按以上图片I=Qg/td(on)+tr和I=Qg/td(off)+tf算下来的电流区别还很大,I=Qg/Ton,这边的Ton是按什么算?
问题2.MOSFET参数Vgs th-栅源极阈值电压5V,Vgs - 栅极-源极电压30V,选驱动芯片的驱动电压最小为多少,最大为多少V?
问题3.MOSFET的耐压值400V,电流Id为17A,满足这条件的MOSFET常用型号有哪些?
1.‘其实峰值电流可以用VCC供电除以驱动电阻来得到,如果通过Qg/Ton, 这个应该是平均电流’,请问您说的VCC指的时MOSFET还是驱动芯片的供电,Qg/Ton的Ton具体指的时开关管datasheet的什么参数?
2。您说的一般驱动电压12V比较合适,驱动芯片电压最小值和最大值的范围是多少适用12V的驱动电压,我看不同的驱动芯片有的驱动芯片电压最大20V,30V等等,这些12V都适用吗?
谢谢
Hi
也注意选择Qg尽量小的,以及MOS的散热也是要注意的。