想请问下,并麻烦您TI的工程师们,我现在使用2路TYPE-C在投影机上,带电池充电,有USB3.1的功能,还有DP显示的功能,外接电脑或手机进行DP显示,这些我都选好型了,原理图我也整合在一起了,使用TPS65987D+TUSB1064这个使用各2PCS,因为有2个TYPE-C端口,一个进行充电,一个进行USB3.1或DP显示,那么,这需要有输入20V5A的电压,输出为5V3A 向外部U盘供电。而这2路TYPE-C的端口,分别对BQ25713锂电池充电,充电管理IC我只用了一路,1PCS,我的问题是:2路TPS65987D向充电管理IC交替提供输入,而与BQ25713的I2C端口以及GPIO端口可以并联在一起吗,还是有别的方法,因为,BQ25713充电管理IC要向TPS65987D提供反馈信熄,充饱或其它充电状态信息,请问应如何接法。
充电管理IC:BQ25713有PROCHOT,CHRG_OK EN_OTG I2C(SCL_1 SDA_1)分别反馈到TPS65987D,但是,我有2个TPS65987D(2个TYPE-C端口)进行PD协议,指向一个充电管理IC,外接4节锂电池,请问应如何处理是好,提前谢谢!