请求指点 :产品有60%以上的线路板产品有故障,经过工程师分析为TI 5430芯片故障,无意中拆下来又焊接到线路板,问题症状消失,然后又测试了十几台,都这样,但是即使好了,芯片问题的根本原因没有找到,设备上电,14V输入端(VIN)接地,把TPS5430焊下来,重新焊接,片子正常工作
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
麻烦高手请指点:出现上电不能正常工作的问题,经过查验发现是芯片TPS5430导致,发现问题的设备芯片生产批号为:5430-TI-16H-ZE28G4, 5430-TI-16H-ZDV4G4。
工作环境:无线发射器,14.4V电池供电,线路板为贴片机焊接。
芯片功能描述:芯片TPS5430,作用是将14V转换成5V。
问题描述:TPS5430芯片的VIN引脚(14V)与GND短路,导致设备不能正常工作。补焊芯片引脚仍旧不能正常工作。将芯片焊接下来,重新焊接上去能够正常工作。另外换用其他型号的芯片,没有发现此类问题。