我用tps610992升压设计,输入电压使用1Hz的正弦信号源,Vpp=1V,偏置0.5V,即0~1V的输入,用示波器发现,输入居然被钳制到0.5V,怎么回事?有输出,不到2V。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我用tps610992升压设计,输入电压使用1Hz的正弦信号源,Vpp=1V,偏置0.5V,即0~1V的输入,用示波器发现,输入居然被钳制到0.5V,怎么回事?有输出,不到2V。
Hi
这个芯片并不是和0~1V的正弦波输入,因为芯片仅仅在0.7V输入以上才能升压。
如果你的设计就是要输入0~1V,那么芯片会在高于0.7V时工作,低于0.7V时不工作。
输入并不是被嵌位到0.5V, 而是你输入本身0.5加上0.5Vpp的正弦波,所以测出来可能就是0.5V,如果用示波器测,电压就会比较准确。