This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq28z610在EVM开发上面测试放电可以从100%放到0%,将烧录文件烧录到自己的主板测试放电电量有跳变



在bq28z610EVM开发上面做循环学习测试,导出量产文件后,烧录到自己的主板测试放电,发现电量有跳变,有一次放电到8%时电量突然跳到0%,另外一次放电到3%时突然跳变到0%,跳变的原因是电池电压已经降到终止电压6.2V,在开发板上面测试没有这样的问题(当电量0%时电池电压约6.9V)。

怎么解决这个问题?