通过GD32F103与CSD97396Q4M相连。GD32F103输出电平为3.3V,CSD97396Q4M连接关系如下图,GD32有输出PWM波形,但测得CSD97396Q4M输出引脚(SW)无输出。SKIP引脚拉低,或拉高都没有输出。将SKIP与GD32断开,测得电压1.5V左右,应该可以说明VDD电压已经进入芯片。芯片自身有一些为降低功耗的功能,没看明白。不知道是不是造成这个现象的原因?因为不想考虑散热,负载电阻采用的是3.3k
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
通过GD32F103与CSD97396Q4M相连。GD32F103输出电平为3.3V,CSD97396Q4M连接关系如下图,GD32有输出PWM波形,但测得CSD97396Q4M输出引脚(SW)无输出。SKIP引脚拉低,或拉高都没有输出。将SKIP与GD32断开,测得电压1.5V左右,应该可以说明VDD电压已经进入芯片。芯片自身有一些为降低功耗的功能,没看明白。不知道是不是造成这个现象的原因?因为不想考虑散热,负载电阻采用的是3.3k
电感22u,电容528u。我测了一下,发现boot电容电压很低,不到1v,boot电容为0.1u。开关频率100k。
请问,您们能根据100k的开关频率,提供合适的boot电容,电阻值吗?输入24v,开关频率100k