This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

变压器驱动,隔离电源

Other Parts Discussed in Thread: SN6501, TPS55010

目前需要一个隔离的5V电源,已有没有隔离的5V。之前采用模块设计(24转5V,隔离),但现在想用1:1的变压器来转,将未隔离的5V转隔离5V。因为之前没有做过这部分,在网上找到的相关资料很少,希望可以有个方法。(看网上资料,大概是需要变压器驱动器驱动的,电流的变化才会有电磁感应),后面转的5V电源,会再转3.3V给STM32供电,所以电流尽量在0.2A左右,看到TI的sn6501 ,但是次级输出电流看手册不是很明确,到底可以达到多少(我理解的100mA),如果是100mA应该是不够用的。

现问题如下:

1.隔离电源,变压器驱动器+ 1:1的变压器是否可行;

2.如果可行,sn6501转隔离后的电流是否满足需求;

3.如果sn6501次级输出电流不能满足要求,请推荐一款芯片;

芯片成本不希望太高,尽量不要超过采用隔离模块的价格(目前采用的隔离模块价格:20RMB)