使用TPS5450翻转负压后由于输出电流3A,过热马上就进入打嗝模式。像这种贴片的芯片有散热片吗。为什么同样的使用,正压就没有这么热
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用TPS5450翻转负压后由于输出电流3A,过热马上就进入打嗝模式。像这种贴片的芯片有散热片吗。为什么同样的使用,正压就没有这么热
Hi
你的输入是多少?注意做成负压之后,最大输出电流是5A(1-D), D是占空比。 同时峰值电流也会比buck时大。 所以选择电感也要注意(饱和电流需要足够)
如果上述都没有问题,再考虑芯片本身功耗造成的温度注意建议用4层板来做,利用中间层大面积的铜箔来散热。芯片底部PAD充分与PCB铜箔焊接,并在正面也做扩展。
(芯片底部的PowerPad就是散热片)
1.对,这也是一个问题,仿真的时候输入15V就行。但是实际输入25V才可以输出-14V电流也是到不了3A;如果小了输出就只有0~-5V。
2.电感选取6A的应该没问题
3.四层板太过奢侈,如果不用的话怎么实现降温,把PAD接出来个散热片吗
正转负压时压差大了,且占空比不一样了,当然会比较热,建议你在Thermal pad以及SW节点上上大面积覆铜