要求:
电源降压芯片.
用在手持式的数据采集器中,IC的封装不能太大.
输入电压是两节Li电池(电压8.4V).
输出电压为3.6V,在最大电流为2A或者3A,转换效率94%以上.
工作在最小电流1mA是的,转换效率也要高,最好有80%以上
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
要求:
电源降压芯片.
用在手持式的数据采集器中,IC的封装不能太大.
输入电压是两节Li电池(电压8.4V).
输出电压为3.6V,在最大电流为2A或者3A,转换效率94%以上.
工作在最小电流1mA是的,转换效率也要高,最好有80%以上
你好,建议使用TPS54320,集成MOSFET,14QFN整体封装大小为3.65*3.65*1(mm)
TPS54320的空载电流<1mA,最大只有0.8mA。内部集成57/50毫欧的MOS,能满足您的需求。