如题.我上次的电流设计只能到2A电流,用的是54260,现在想改成40060不知道行不行.
大神们...我爱TI,我爱你们.告诉我吧.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我估计你的问题出在了频率设计这里,你电路的频率是可以由你自己设定的,在例子里,由于输出电压太低,占空比很小如果选择频率过高上管导通时间将很小,会小于技术规格书里那个电流延时(大概是这个意思,没细看)也就是说MOS管导通必须有一个最小时间,不能小于330nS,所以他才根据这个指标来设计的频率(如果他选择频率150K,占空比0.058,导通时间将只有280nS也就小于330了)而对于你来说不存在这个问题,你输出电压很高,最小占空比也很大,所以你选择100K还是200K都是可以的,这个由你自己决定。然后你再去计算上管的损耗试试。
不知道我说的你是否明白?