我现在的系统是24V输入,但是需要设计一个输出范围从10V到60V的电源输出。最大电流1A@60V就足够了。而且要能够保证输出是可以开关的。
【之前用LM3488设计了一个DAC和FB串联控制的Boost电路,在调节电压时,MOS管莫名其妙的烧掉了。现在根据需求准备重新设计电路。】
现在的思路是使用DCDC隔离电源方案或者用Buck-Boost/***。输入电压实际是不变的,但要求可以通过MCU的DAC或PWM,甚至数字接口控制输出变化。
有没有什么好的器件推荐,以及怎么用来设计。(LT5118能实现吗?还是智能用隔离电源的方式?我是电源设计的新手,请多担待。)