This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MAX1724EZK50-T



大家好:

       由于实验室需要,目前需要尽快得到3.6V电池供电生成+-5V输出电压的低功耗(Iq为uA级别)、输出电流最大能够达到60mA、小纹波的电源方案。碰到了一些问题: 

1. 使用MAX1724EZK50-T推荐电路,3.6V电池供电,产生5V电压,接上负载150欧姆后,电压会被拉低到4V,推测是输出电流不够大。电感使用的是推荐值10mH,但是用的是普通的贴片式电感。请问电感的型号对于带负载能力会有影响吗?我该如何改善带负载能力呢?

2.大家还有哪些像MAX1724EZK50-T这样的3.6V供电,低功耗,输出电流能够达到60mA的-5V电压生成方案呢?

      题主是机械专业的,搞电路也是新手,希望大家能够帮助我~谢谢大家~