This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24133 LED灯一直闪烁



 请教一下,我使用的这个电路图,15V输入,充12.6V锂电池正常。现在的情况是我做了另外一块电路板,想充一节电池(4.2V),我将cell引脚接地,然后电压输入改成5V。调试时出现LED一直闪烁,测试过VREF=3.3V正常,但是SW电压才有2.9V。所以请教一下,这样改原则上可不可以?

  • Vcc至少需要升到5.2V或D3换成肖特基才能正常。

    由于AVCC最低工作电压4.5V,3.8V即欠压。考虑到D3可能有1V压降和线损,而这个压降是随电流而变的。这样;每回IC启动--消耗电流增加--D3支路压降增大--欠压--D3支路压降降低而AVCC电压恢复正常启动--IC消耗电流增大--D3支路压降增大--IC欠压。。。如此;欠压再重新启动再欠压的循环打嗝,LED也因此闪烁。
    因此;减小D3支路压降或提高输入电压;避免AVCC欠压就可以避免故障。
  • Hi
    输入电压提高,问题是否消失?