This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

确定TPS61230上电时间



现在想用这个IC对模块供电,模块对供电的要求是,输入电压5伏,输出有两个,一路是3.3V,一路是5.5V,对上电时间(就是输出电压从10%到90%)要在0.5ms 到10ms,下电时间要在10ms以内,电流在1A以内。我们看了spec,这个芯片的上电时间有三段构成,不好确定,现在想请教一下,谢谢!