This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65218D0 RTC切换纽扣电池供电问题

Other Parts Discussed in Thread: AM4379, TPS65218D0, TPS65218

TI的老师们:

         你们好!

      我用TPS65218D0作为AM4379的电源管理芯片,现在遇到这种情况,当外部5V通过IN_BU供电的时候,DCDC5/DCDC6都有1.8V和1.1V输出,SYS_BU也有5V电压输出,当我关闭外部电源的时候,有时候会导致纽扣电池切换不正常,CC引脚有电压,但SYS_BU没有输出,DCDC5/DCDC6也没有输出,后来发现好像是PWR_EN没有1.8V输出,导致PMIC没有工作,在直接纽扣电池的情况下,我直接上拉PMIC引脚,DCDC5/DCDC6都有输出了,SYS_BU也正常,RTC晶振起振,但是一断开PWR_EN的上拉,又没输出了,有时候又会莫名其妙的好了,RTC掉电也能走,抠下纽扣电池再装上,DCDC5/DCDC6还是有输出,然后我把纽扣电池抠下来的时候,CC引脚上的电容短接一下,上上去又不行了,请问这种是什么情况引起的?不是只要RTC起振PWR_EN就会输出1.8V高电平吗,AM4379处于RTC_Only模式。电源部分和参考的一模一样,TPS78101也没用,用的DCDC6,电阻焊上的!Am437x_gp_evm_3k0006_schematic_rev1_4a.pdf