This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5176启机及关机问题

Other Parts Discussed in Thread: LM5176

LM5176启机及关机问题讨论及分析

  1. 应用背景介绍:针对LM5176的功能设计,应用在buck-Boost加全桥变压器隔离的模块电源上,其中后级全桥变压器为开环架构。具体如下框图:

 

 

 

 

 

 

 

 

 

 

 

 

 

如上图例,在此设计中实际测试出现如下问题:

  1. LM5176内部的误差放大器是跨导型的,以前没接触过这种类型,查资料自己体会到的是,跨导描述的是输出电流Io与输入电压Ui的关系:gm=Io/Ui  按量纲应该是ohm^-1,规格书里给的是mS,这是为何?
  2. 跨导型的误差放大器的传递函数是什么样的?即外围FB引脚,COMP引脚搭建的RC电路存在着什么样的关系?(现在遇到的问题与控制参数有关)
  3. 测试异常波形图如下:

(黄色:输出28V   绿色:ss引脚    紫色:COMP引脚    红色:Boost-Mos驱动)

    36V启机异常波形:启机上升过程中输出电压有震荡

 

 

 

 

 

 

 

48V启机异常波形:启机上升过程中输出电压有震荡,且有跌落

 

 

75V时启机波形正常:

 

 

 

 

 

 

 

 

75V关机波形异常:

 

 

48V关机波形正常:

 

 

36V关机波形正常:

 

 

 

附图:

LM5176原理框图

 

 

 

启机异常包括两个:一个是36V,48V启机时输出有震荡,另外就是48V启机时有跌落。

最开始36V,75V也是有跌落的,调整了控制参数:SLOPE引脚电容参数变大就好了,但48V跌落只是没之前那么厉害,现在又引入了震荡,请问控制参数往哪方面调才能解决?

75V关机出现跌落时候刚好是随着输入电压的下降,Buck-Boost由buck模式切换到Boost模式过程中出现了空挡,这个是控制引起的吗?