This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25895无法实现对电池4A充电

Other Parts Discussed in Thread: BQ25895

Hi:

    我们这边电源适配器,输出3.6V-6V/3A, 6-9V /2A, 9-12V /1.5A适配器,充电IC用的BQ25895,,对3.4V 4000ma的锂电池充电,全部接好后,

    USB接口最大输出电压12.2V,700mA对锂电池充电,调整寄存器,电流达不到1.5A。

读出的寄存器:

设置04寄存器为40,电流从0.7A变为0.8A,没有到1.5A,无法大电流充电,请问是什么原因?