This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24073的异常过度充电,不受控问题。

Other Parts Discussed in Thread: BQ24073, BQ24074

设计中由于存在压降损耗,导致到BQ24073的VIN端的电压只有4.3V了,这时电池Vbat端电压为3.8V,芯片还算正常,没有异常充电;

但是当Vbat电压到达4.17V时,芯片就会开始向电池充电,电流47ma(符合设计的充电电流),Vin电压掉至4.23V。如果此时继续升高Vbat,充电电流会越来越小,Vin也有一定的升高。

整个过程中,充电使能CE和充电指示CHG都是高电平,没有变换,即芯片判断是没有充电的。

最终电池电压被充到了4.23V左右,过充了。充电芯片不受控。

请问这是什么原因导致的?内部是什么通路被打开了吗?