This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS50601电源芯片测试



TPS50601测试过程中,
不适用SOCKET,直接焊在PCB上,芯片没有问题;
使用SOCKET后,VIN和PVIN 不能连接在一起,PVIN能够达到6V,VIN在超过4.4V以后,芯片不能正常工作;不正常现象是:SS/TR引脚成锯齿波,升上去到一个电瓶后立马被拉低,此时负载为165mA,(现在的PCB上的器件参数和不使用socket的一样)。  


这时候的原因可能是什么?

1、环路参数不匹配? 如果不匹配,该改那些参数?(在此之前改过SS/TR引脚的电容,COMP处的阻容,都无改变)
2、PCB噪声?  如果是这个,那就很.......
3、  或许还有什么原因???