This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A8101低温自激

Other Parts Discussed in Thread: TPS7A8101

我们正在使用TPS7A8101,发现部分芯片在温度达到-20℃以下时,芯片就会产生异常信号,怀疑是自激(400kHz左右,幅度大概为50mV),当温度升高至10℃左右,信号消失。

把Cbypass由100nF减小至100pF,情况有所改善,但是温度继续降低到-30℃,异常信号又会冒出来,请问该怎么解决?该器件能通过仿真确认吗?

应用场景:Vin=3.65V, Vout=3.3V, Iout=30mA.

x 出现错误。请重试或与管理员联系。