Other Parts Discussed in Thread: TPS61500
我在使用时,电源为3.7V锂电池,设置的是350mA的电流,输出端接一个3.3V的LED可以输出3百多电流,但是再串联一个LED,电流就降了一百mA,,再串联一个LED,还能点亮,但是输出电流又小了,这个的原因可能是什么?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TPS61500
我在使用时,电源为3.7V锂电池,设置的是350mA的电流,输出端接一个3.3V的LED可以输出3百多电流,但是再串联一个LED,电流就降了一百mA,,再串联一个LED,还能点亮,但是输出电流又小了,这个的原因可能是什么?
电感器是 10uH IND-10104封装 SL01040H100MTT SUNLTECH
ID Name Designator Footprint Quantity Manufacturer Part Manufacturer Supplier Supplier Part
1 TPS61500PWPR U1 HTSSOP-14 1 TPS61500PWPR TI LCSC C71160
2 210k R1 R0805 1
3 13.7k R2 R0805 1
4 0.1u C1,C3 R0805 2
5 10u C2 R1210 1
6 470nF C4 R0805 1
7 1u C5 R0805 1
9 10uH L2 IND-10104 1 SLO1040H100MTT Sunltech LCSC C182194
10 0.39 R3 R2512 1
11 80k R4 R0805 1
14 MBRA340T3G D1 SMA 1 MBRA340T3G ON LCSC C26178
0.001R R1210
0.0005R R1210