This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tps61032输出5V没有问题,但锂电池电压被拉低

Other Parts Discussed in Thread: TPS61032

我根据tps61032的规格书电路图,现在输出5V没有问题,但输出电流在350mA左右时,锂电池电压从3.92V马上被拉低到3.6V或者3.5V左右,请教是什么原因?谢谢

  • 这块锂电池本身没有问题的,在其它非tps61032的板子上表现正常。

  • TPS61032其输出电流的能力,按输入电压3.2V~4.2V,输出5V的方案计算可达2.5A,是否有加大负载电流做个测试?也是同样会被拉低?能否换个电池或者直流稳压源做同样的测试?非TPS61032的板子,其负载电压,电流为多少??

  • 换了电池也是一样的。

    我没有直流稳压源,但我用万用表串入电池正极,测试空载时的电流是正常的,我是用MSP430,在360uA左右。但一加上5V负载,就是给mp4 充电,TPS61032的5V输出还是稳定的,但用万用表串入电池正极,这时mA档的电流已经显示超出了,说明电池输出电流很大,导致电池电压马上被拉低了。


    目前我的板子只焊接了TSP61032升压部分,其它部分没焊。


    我们怀疑TSP61032可能坏了,但为什么空载和带载时,输出的5V非常稳定?

  • 刚才只焊了TPS61032升压部分,没焊MSP430。给mp4充电,锂电池从3.9V降到3.2V,而给数码相机充电,TPS61032直接冒烟。。。

  • 您用的电感感值是多少,饱和电流多大?如果饱和电流过小,加大负载后实际感值会下降,导致电感电流急剧上升,很容易烧功率管。

  • 我用的是TPS61032电路中的6.8uH,12 X 12MM的,电流应该足够了:

    我现在在试LTC1700,外置MOS管的,用了2.2uH的功率封闭电感,7 X 7MM的,目前测试带2个USB 5V负载都没有问题。

    我估计TPS61032比较敏感,容易击穿内部的MOS管。网上也有烧坏的案例。。。

  • 如果您还对TPS61032有兴趣,可以试一下用您现在使用的2.2uH替换原来的6.8uH再做测试。

    另外SW点的overshoot电压过高是会烧下管,而overshoot电压高低和从输出端到输出电容之间引线的寄生电感有关,所以要尽可能将输出电容放在靠近输出引脚的地方。

  • Hi :

       请在输入再增加一个10~22uF的电容, layout上要尽量靠近芯片和电感。

       另外请找其他可以确认饱和电流规格电流进行验证,规格4.7~10uF。