If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The EDV2 threshold is set to the 7% SOC voltage, EDV1 is set to the 3% SOC voltage and EDV0 is set to the 0% SOC voltage. If you are using EDV mode, then these thresholds must be found by analyzing discharge data to determine the value of the parameters to enter into the data flash. If you are using CEDV mode, then the gauge will calculate these thresholds based on the CEDV Coefficients and these must be calculated using the online GPCCEDV tool. The mode is selected with the CEDV bit in the CEDV Config register.