This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC21520DW 驱动 SIC C3M0065100K,400V输入下自举二极管、自举电容损坏,芯片 VDDB、OUTB、VSSB三个管脚短路,是什么原因呢?

Other Parts Discussed in Thread: UCC21520

采用芯片规格书中推荐电路,用于驱动移相全桥逆变,如下所示:

器件选型说明如下:

1   VDD为19V;

2   Rboot=2.2Ω,Dboot型号为US3M,超快恢复二极管,耐压1000V,3A,1.8V;

3 上管自举电容 Cboot=1uF,下管Cvdd=1uF;均为陶瓷电容,型号GRJ21BC72A105KE11L,X7S,100V,±10%,SMD0805;

4  Cz=1uF,型号同3,GRJ21BC72A105KE11L;

5  Vz 型号 BZT52B3V0-E3-08 ,3V;

6  Vz、Ron之间串联5.1Ω电阻;Ron=5.1Ω;无Roff ; Doff 型号为 MBR130T3G,30V ,1A;

7  Rgs=10kΩ,Rgs并联1nF电容;

8  开关管为sic mos,型号C3M0065100K 1000V  35A;

故障描述如下:

1  逆变输入电压370V时,系统运行10分钟,驱动无问题;

2  输入电压增加到400V时,系统运行约4分钟,驱动电路出现故障,损坏现象如下:自举二极管被击穿短路,自举电阻开路,VDDB、OUTB、VSSB三个管脚短路;

3  损坏4次,都是同一个位置的UCC21520DW,其他路UCC21520DW 均正常;其中一次是VDDA、OUTA、VSSA短路;另外三次是VDDB、OUTB、VSSB短路;

问题:

1  关于自举二极管,是最好使用SIC 肖特基才可以吗?尝试US1M、US3M超快二极管均无效果;规格书中推荐型号为C4D02120E,耐压1200V,sic肖特基二极管。

2 是否可能是UCC21520 引脚负压导致损坏?用高压隔离差分探头测试 VSSA 负压尖峰为-2.6V,规格书中引脚电压为-2V~VDD+0.3。

3 如果器件有推荐选型,请推荐下,谢谢!