我用的BQ25703A,现在还没有接CPU,单独调试充电电路,5V电压输入,设置的是两节电池,不接电池时,电压可以升到6.2V左右,带载却只能带0.7A,大于0.7A就会被拉低。
接入电池(电池电压7.6V)后,没能进入到充电状态,充电IC的输出电压也没有高于7.6V,BATDRV仍然输出高电平。电池在位,拔掉USB电源,可以自动进入电池供电状态。
请问这种现象可能的原因有哪些呢?要从哪方面排查?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我用的BQ25703A,现在还没有接CPU,单独调试充电电路,5V电压输入,设置的是两节电池,不接电池时,电压可以升到6.2V左右,带载却只能带0.7A,大于0.7A就会被拉低。
接入电池(电池电压7.6V)后,没能进入到充电状态,充电IC的输出电压也没有高于7.6V,BATDRV仍然输出高电平。电池在位,拔掉USB电源,可以自动进入电池供电状态。
请问这种现象可能的原因有哪些呢?要从哪方面排查?
示波器探头的档位设定是否正确,如果是46V,MOS肯定会损坏了。
请确定一下,
1. USB认别没有问题,USB可以提供足够的充电电流。或者用5V adapter或直流电源来测试看看。
2. Sys是否有其它负载。
3. 充电时,用万用表测试一下R1206两端的电压,看看充电电流是多少?
4. 如何判断电池没有充电成功的?多久测的电压?电池容量是多少,此时电压是多少?