Other Parts Discussed in Thread: LM3409HV, LM3409
我使用我使用LM3409HV芯片很容易发热,工作不一会就会非常烫,使芯片不能正常工作,甚至经常将IC烧糊,有没有遇到同样问题的朋友,如何才能解决这个问题呀,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
如果你采用的是eMSOP-10 Package封装,并且不用case散热(即热阻是50 °C/W), 芯片powerpad充分与PCB GND焊接,并扩展此GND 面积至少2平方英寸,芯片的温度大约是75℃,如果采用的是DIP-14 Package(热阻是87°C/W),因为没有散热的powerpad, 芯片的温度将大约是100℃。建议你采用Junction to Case的方式散热。
Hi:
按照你的参数,扣掉D17, 效率也只有82%,请问能否告知你的MOS名称(电路图中名称的查不到),如果你采用eMSOP-10 封装,layout没有问题,DIP-14 封装,温度比上述高的还要高,就需要确认一下你的MOS, 因为芯片的主要功耗消耗在驱动MOS上,另外,适当的降低频率也可以达到降低温度的效果(稍微增加Roff阻值,电感就要稍微选大一点的,例如330uH,390uH)
您好,我的MOS名称确实写错了,应该是IRF9540N,封装用的是eMSOP-10的,因为听人说DIP14的不好买,其实我更希望用DIP14的。频率我感觉已经很低了,现在只有100KHz左右。我也发现了,效率是不怎么高,如何才能提高一点呀,Junction to Case的方式散热如何实现呀,这方面没有接触,谢谢您了
Hi
您的MOS Rdson 117mohm太高了,会严重的影响效率,或许您可以选择SUM110P08-11L或者类似规格的MOS, 他们的Rdson大约12mhom(MOS功耗减小接近10倍).
Hi
注意一下,电感也要选择ESR较小的电感,这个也很影响效率,D17的Vf也要尽量选小一点的。
Hi
见Vcc电压描述:the steady state VCC pin voltage is typically 6.2V below the voltage at the VIN pin. The VCC pin should be bypassed to the VIN pin with at least 1μF of ceramic capacitance connected as close as possible to the IC.
VCC的与Vin之间的电压压差典型的是6.2V, 这个电压并非针对GND, 请注意。
我测了两个,VCC与VIN间电压一个是6.059,一个是6.086,应该没有问题吧,
Hi
是的 6V是正常的。
如果芯片在75℃是正常的,太高就不正常,TI没有出junction to case的具体设计方案,这个您可能要在网上找。
之前提到的MOS, 请注意。
您好! 我也选用过SUM110P08-11L这样的MOS,但一接上电源就频闪,是不是因为它的Qg太高,还是因为的开关延迟时间太长?
我用的比较好的是IRF9Z34,但同样发热量比较高!