This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570BMS设计



我在电源管理方面是个新手,我想在你们MS570BMS的基础上设计符合我需要的电源管理,因为我需要的是为我们实验室的一个小型的电动小汽车进行供电和实现电源管理,所需要的电池电压为48 V容量为20AH,一般的锂离子电池的工作电压为3.7v容量为2000mah,因此我需要选择额13串10并的连接方式组成电池组供电。我看了你们官网上的示例的是串联16节电池,所以我想知道是你们的TMS570BMS的设计方案是不是也可以实现对串并联电池组进行电源管理的?

1.如果采用你们的EM1402EVM均衡评估板,我想知道的是你们这个板子均衡的依据是什么?是依据电池的电压吗?

2.如果均衡的依据是电池的电压,那按原理分析的话按照我需要的48V20AH的需求的话,是13串10并,也是可以实现的吧!因为虽然我需要的电池组中的电池连接方式是既有串联也有并联的,并联只是增加电池组的容量,不改变电压,只需要监测13节串联起来的电池即可对吗?

3.当然如果我只连接13节电池串的话,必然不可能实现每节电池单体的监测但应该是可以确定哪一串的电池组出现了问题对吗?

谢谢解决!