Other Parts Discussed in Thread: BQ24072, TPS7A05
当使用适配器和电池同时供电时,实测VBAT是3.96V,实测VOUT是4.2V,跟手册中一致。
但是当电池拿掉,只使用适配器供电时,实测VOUT是4.44V,跟手册中的3.5Vmax值不符。
排查时,检测到VBAT脚电压波形如下,幅值2.2V,频率1.85Hz:
4.44V输出已经超过了我们负载芯片的最大额定值,存在损坏芯片的风险。请问这是什么原因导致的,以及如何解决,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.