This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65130输出极限值正负15V是否有问题?

Other Parts Discussed in Thread: TPS65130, TPS65131

现在我打算采用TPS65130输出正15.3V(50mA),-15V(50mA),
模拟负载测试输出电压与纹波正常,但芯片推荐输出最大值分别为+15V,-15V,长期工作,芯片是否有失效的风险,需要专家确认?谢谢!
  • Hi

        TPS65130正负最大输出推荐+/-15V, 原因是VPOS/VNEG的最大耐压是+/-17V, 故即便您的正输出达到了15.3V也不会有问题(建议您确认其纹波,让其尽量小,反馈电阻也尽量采用高精度电阻1%或者更高,另外测试一下空载启动等等,需要在任何情况下VPOS电压不要高出15.5V被推荐)

  • 谢谢johnsin的答案及建议,TPS65130电源用于驱动CCD的容性交流负载,纹波现在还没模拟测试。另外改用TPS65131,在输出+/-15V时输出电流更大。

    johnsin,能留个邮箱嘛,以后调试有什么问题请教你。