This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MOSFET驱动器LM5101A使用使用上有几点疑问

Other Parts Discussed in Thread: LM5022, LM5101A

我这样使用LM5101A:PWM控制器+LM5101A+功率MOS,电路跟LM5022手册中推荐的典型电路差不多(PWM控制器不用LM5022),只不过是在PWM和MOS之间再加一个LM5101A,加强一下mos的驱动能力。只使用LM5101A的low side驱动MOS功能,不用high side。问题来了:

1、不用high side时,引脚HO怎么处理,可否悬空?引脚HI怎么处理,可否接地?、

2、LM5101A手册figure25典型应用电路中,既然不用high side了,那么HO和HS之间的自举电容Cboot还需不需要?

3、引脚VDD供电电压是否就是LO(HO)电压(门驱动电压)?

4、LM5101A手册figure25典型应用电路中,在低频100K条件下使用LM5101A,那么自举二极管Dboot是否需要?如果不用Dboot,那么自举电阻Rboot是否需要?

5、在LM5101A手册第一页的Description中写到‘The floating high-side driver is capable of operating with supply voltages up to 100 V‘,请问这个’ floating high-side driver‘怎么理解?’supply voltages up to 100 V‘这个100V指的是什么,是high side mos的D端电压吗?

6、LM5101A分为TTL和CMOS,请问怎么选择?跟PWM驱动器是数字或模拟类型有关吗?如果有关,请问怎么判别PWM驱动器是数字的还是模拟的?

7、LM5022的引脚pin5OUT输出电压是多少(也就是门驱动电压)?在手册中没找到