This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54335A电源最大输入最大电压确认

Other Parts Discussed in Thread: TPS54335A

你好: TPS54335A 资料显示最大输入电压为:30V;可是我选择的TVS 1.5SMC27A其钳位电压达到了37V了, 所以应该起不到保护TPS54335A的功能了;可是为什么没有出现毁坏TPS54335A现象呢? 是不是TPS54335A能承担的输入电压会更大?

  • 30V是保证你绝对不会损坏的电压,超过30V可能不损坏,但不能保证不损坏。就好比50V电容,你可以加55V电压使用,但出了问题,电容厂家不负责。

  • 首先;这是个例。不是每个器件耐压是一样的。
    其次;那是工作电压而非实际耐压。如同你能举100kg,当让你举着100kg跑步;就是另一个概念了。
    再其次;厂家保证有最低的最高工作电压。为保证所有产品都能满足;所有产品都需要预设冗余而保证100%合格。
    所以;一两片的耐受量并不等于其它都能耐受。高于额定值也不一定意味损坏。
  • Hi
    就设计而言,TVS建议选择低一点,如你所说37V起不到保护作用。
    超过30V,就有烧的风险,但是略高,不一定会烧。
  • 手册上标注的recommand电压是指在芯片能承受DC 28Vin, Max是指芯片能承受的AC电压最大到30。在以上条件下,芯片都没有问题

    对于你37V没坏这是随机事件,和实测应用条件有关,所以建议你降低TVS管的电压在芯片可承受范围内,以防损坏